Part Number: DS80PCI402
Hi,
I need to determine how to operate the repeater with a downstream device that does not support RXDET. In my setup, DS80PCI402 is operating as a SMBus slave device. PRSNT pin “active”, RXDET = “1”?
Table 4 of datasheet does not match text in datasheet. PRSNT pin is “active” when a downstream device is installed. I have the RXDET external pin with 1K pullup.
Table 4 from datasheet has a RXDET column and a Bits [3:2] column. I presume that this is referring to reg addr 02, but Table 9 calls these bits RESERVED. Is the RSDET column ORed with the BIT 3:2 column? Does one column override the other?
Please advise -- thank you.