Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS110DF410: does DS110DF410 support 3.125Gbps datarate?

Part Number: DS110DF410
Other Parts Discussed in Thread: DS125DF410

Hi ,

in customer's application, DS110DF410 needs to communication with 2.5G optical module, the datareate of optical module is 3.125Gbps.

in test, communication fails,

so customer want to check if DS110DF410 supports 3.125Gbps datarate?

thanks.

  • Hi Max,

    The VCO of the DS110DF410 can only support data rates ranging from 8.5-11.3 Gbps and divide-by ratios of 2, 4, and 8. Looking at the 3.125 Gbps data rate, the DS110DF410 VCO will be unable to lock to this rate.

    A more suitable choice is the DS125DF410. This device's VCO supports data rates ranging from 9-12.5 Gbps and divide-by ratios of 2, 4, and 8. With the DS125DF410, you can set the VCO to lock to 12.5 Gbps and a divide-by ratio of 4 to achieve lock at 3.125 Gbps. For more information, please see the DS125DF410 datasheet, Table 2 for "Standards-Based Modes Register Settings" for commonly supported Standards.

    Thanks,

    Michael