Part Number: TLK1501
Hi!
In the datasheet on TLK1501 it is said that the built-in 8b / 10b encoder automatically generates the sequence K28.5, D5.6 (K28.5, D16.2). According to the FibreChannel standard, this sequence should be K28.5 D21.4 (K28.5 D21.5). Therefore, there are questions:
1. Is it possible to change the byte D following the K-symbol?
2. Is it possible to bypass the built-in encoder and feed to the input 20 bit words (already passed encoding)?