This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DP159: about register setting for SN65DP159

Part Number: SN65DP159

Hi dear supporting team,

customer want to get all the regs setting needed of below two working mode for SN65DP159:

1. as HDMI retimer

2. DP retimer

could you pls help provide it? tks a lot!

  • Hi Vera,

    The SN65DP159 is designed as a DP++ to HDMI retimer / redriver. It does not function as a HDMI retimer.

    There is an application note that describes the requirements for using the SN65DP159 as a DP to DP retimer. Please be aware that this mode requires an FPGA or similar to actively check and set the regsiters: www.ti.com/.../slla358.pdf

    Regards,
    JMMN