This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB7320: TUSB7320 / USB3.0 compliance test procedure

Part Number: TUSB7320
Other Parts Discussed in Thread: TUSB7340

Hi,

The customer plan to perform USB3.0 compliance test, then can they perform it without PCIe and JTAG control? They'd like to perform it with only GRST# input and CLK input. 

Best Regards,

Satoshi / Japan Disty

  • Hello Satoshi,

    Please note the TUSB7340 is NRND and it will not pass USB compliance certification tests.

    Regards,
    Roberto
  • Hi Roberto,

    I found some thread abut TUSB732x and I understand that it's difficult to pass USB3.1 compliance test. But now I'm talking about USB3.0, so can you give your comment for following question?

    • Can they perform it without PCIe and JTAG control? They'd like to perform it with only GRST# input and CLK input. 

    Best Regards,

    Satoshi

  • Hi Satoshi,

    The TUSB7340 is compliance with the xHCI 0.96 spec. Also, you'll require the PCIe to pass the compliance tests described in usb.org as electrical, interoperability, CV test, etc. since some of these tests requires that the device be fully functional.

    Regards,
    Roberto