This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB7340: ABS MAX limits on OVERCURx_N inputs

Part Number: TUSB7340

Customer has mistakenly tied OVERCURx_N input to 5V via a 3.3K pull-up.  This violates the ABS MAX limit of VDD33 + 0.5V.  Customer has a number of systems in the field and wants to understand the risk of damage to the device under these conditions.