Part Number: TPS65982-EVM
Other Parts Discussed in Thread: TPS65982-EVM, HD3SS460
Dear All,
I am currently testing several USB type-C to C male cables and all is working fine, But to complete my testing I need to benchmark the Bandwidth of the cables up to USB 3.1 gen2 up to 10Gbps. Can I use 2 or more TPS65982-evm and a FTDI or Aardvark to benchmark the bandwidth speed of the cable.
First question is this possible?
Second question what do I need to do?
Kind regards,
Mitchel Rietdijk