Part Number: TFP410
The datasheets states that the input pixel clock may range from 25 - 165 MHz. Now, I wonder if this specification is also true for 12-bit DDR input mode. My actual question is if it is possible to use the 12-bit DDR input with a 1080p60 video signal, which implies a 148.5 MHz 12-bit DDR input, or if only around ~82.5 MHz 12-bit DDR is possible?
Thanks!