Part Number: DS90UH925Q-Q1
Hi,
I would like you to confirm about below.
* Could you please tell us "min" time from "VDDIO/VDD33" to "PDB" ?
I understood that "max" time from "VDDIO/VDD33" to "PDB" according to following sentence of datasheet.
"The VDDs (V DD33 and V DDIO ) supply ramp should be faster than 1.5 ms with a monotonic rise."
However, there is no description about "min" time.
According to DS90UB921, this "min" spec is defined as "0.05ms". Can we apply this spec to DS90Ux925 as well ?
Best Regards,
Machida