Part Number: TUSB422
I have a design which is powered from the VBUS rail on initial cable insertion the sink profile is negotiated correctly:
________ _________ ____ ___ ___
/_ __/ / / / __/ _ )/ / /|_ ||_ |
/ / / /_/ /\ \/ _ /_ _/ __// __/
/_/ \____/___/____/ /_//____/____/
PD Stack v0.98
=====================================
TCPM Init
UNATTACHED_SRC
Port[0]: addr: 0x20, DRP, Rp: 3.0A, Flags: Try-SNK.
VID: 0x0451
PID: 0x0422
DID: 0x0100
REV: 0x02
PD Init
TUSB Init Complete
CC status = 0x13
ATTACH_WAIT_SNK
CC status = 0x13
ATTACHED_SNK
tcpm_hal_vbus_enable(port, VBUS_SNK);
PE_SNK_STARTUP
tcpm_mux_controlMux: USB
PE_SNK_DISCOVERY
PE_SNK_WAIT_FOR_CAPS
PD Rx
PE_SNK_EVALUATE_CAPABILITY
PE_SNK_SELECT_CAPABILITY
PD Rx
PE_SNK_TRANSITION_SINK
tcpm_hal_vbus_enable(port, VBUS_SNK);
PD Rx
PE_SNK_READY
PD Rx
PD Rx
PD Rx
PD Rx
PD Rx
PD Rx
PE_SNK_EVALUATE_CAPABILITY
PE_SNK_SELECT_CAPABILITY
PD Rx
PE_SNK_TRANSITION_SINK
tcpm_hal_vbus_enable(port, VBUS_SNK);
PD Rx
PE_SNK_READY
Policy Engine State History:
[0] SNK_STARTUP
[1] SNK_DISCOVERY
[2] SNK_WAIT_FOR_CAPS
[3] SNK_EVALUATE_CAPABILITY
[4] SNK_SELECT_CAPABILITY
[5] SNK_TRANSITION_SINK
[6] SNK_READY
[7] SNK_EVALUATE_CAPABILITY
[8] SNK_SELECT_CAPABILITY
[9] SNK_TRANSITION_SINK
->[10] SNK_READY
Type-C State: ATTACHED_SNK (last: ATTACH_WAIT_SNK)
Then the device is power cycled (This causes VDD and VCONN to cycle on TUSB422) but MCU remains on and cable remains inserted. With the power cycle I am re initializing the SW stack. During this time there appears to be a hard reset on CC. This results in the SW stack getting stuck in the discovery state and the incoming Source_Cap massages are ignored :
________ _________ ____ ___ ___
/_ __/ / / / __/ _ )/ / /|_ ||_ |
/ / / /_/ /\ \/ _ /_ _/ __// __/
/_/ \____/___/____/ /_//____/____/
PD Stack v0.98
=====================================
TCPM Init
UNATTACHED_SRC
Port[0]: addr: 0x20, DRP, Rp: 3.0A, Flags: Try-SNK.
VID: 0x0451
PID: 0x0422
DID: 0x0100
REV: 0x02
PD Init
TUSB Init Complete
CC status = 0x13
ATTACH_WAIT_SNK
ATTACHED_SNK
tcpm_hal_vbus_enable(port, VBUS_SNK);
PE_SNK_STARTUP
tcpm_mux_controlMux: USB
PE_SNK_DISCOVERY
PE_SNK_WAIT_FOR_CAPS
PE_SNK_HARD_RESET
PE_SNK_TRANSITION_TO_DEFAULT
tcpm_hal_vbus_disable(port, VBUS_SNK);
PE_SNK_STARTUP
PE_SNK_DISCOVERY
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
CC status = 0x13
tcpm_hal_vbus_enable(port, VBUS_SNK);
Policy Engine State History:
[0] SNK_STARTUP
[1] SNK_DISCOVERY
[2] SNK_WAIT_FOR_CAPS
[3] SNK_HARD_RESET
[4] SNK_TRANSITION_TO_DEFAULT
[5] SNK_STARTUP
->[6] SNK_DISCOVERY
TCPC-0 Regs:
10: 00
11: 00
12: ff
13: 0f
14: ff
15: 7f
18: 60
19: 00
1a: 0a
1b: 06
1c: 60
1d: 13
1e: 00
1f: 00
2e: 02
2f: 00
70: 00
71: 00
72: 00
73: 00
74: 00
75: 00
76: 00
77: 00
78: 00
79: 00
90: 00
92: 00
94: 04
A0: 00
Based on the register dump it looks a little like the Hard Reset brown-out has caused the TUSB422 to reset, but not the MCU.
Power Tree
VBUS ---------3v3---MCU
\----5v--------3v3----TUSB VDD
\-----------TUSB VCONN
Is there a way to recover from this (I imagine if I re init the stack I will find myself deadlocked)?
Or maybe is there something I should be calling before I re initialize the stack to prepare the TUSB422?
Note: I am using rev 0.99 of stack despite header printout.