Part Number: DS90UR910-Q1
Tool/software: Linux
Hi All,
We are using DS90UR910-Q1 chip. External video source output board giving input signals on RIN+/-.
We are actually probing the LOCK and PASS pin using Bitscope BS10u. We are getting always logic '0' (means low level)
- LOCK pin (no-24)
- Status: It shows logic '0' --> which means PLL is unlocked
- PASS pin (no-25)
- Status: Its shows logic '0' --> which means PASS = 0: Indicates an error condition or corruption in display timing
Is our observation right ?
What could be the possible reason ?
We have also probed RIN+ & RIN- pins as well , where getting correct signals.
Please reply with suggestion, that will be very helpful to us.
-Ankit.