Part Number: TPS2033
Hi community,
We are using the TPS2033D as a current limiter in an USB implementation.
The ENable pin of the TPS2033D is constantly pulled high to 3.3V as soon as the device is powered up.
As a test, we connect a variable resistive charge to the USB VBUS (5V) controlled by the chip outputs.
After power-up, we increase the output current sinked by the resistive load from 100mA to 3.5A.
According to our understanding of the datasheet contents, we expected the chip to limit current at around 2.2A (2.7A at most), but this only happened over 3A.
What did we miss in the datasheet interpretation?
Thanks in advance for your support.
Mathieu.