Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS25BR110: DS25BR110 - Camera link repeater

Part Number: DS25BR110

Hi Team,

Can you please help with finding a device for Camera link repeater with at least 500Mbps and part to part skew no more than 200ps?

I want to use DS25BR110 LVDS Buffer with Receive Equalization.

The device have 2 pin of equalization.

I use data a rate of 500Mhz.

I need help what to do with 2 pin of equalization.

I’m doing a simulation with DS25BR110 and I can’t understand how to determine the configured equalization.

Is it configurable at all in the IBIS model? If not, what is the equalization that is used in the model?

Thanks,

Shlomi

  • Hi Shlomi,

    There is not much equalization gain available to just 500 Mbps.  The input equalization is optimized for 3 Gbps operation.

    Unfortunately the IBIS model does not include the ability to simulate for equalizer settings.

    How much attenuation do you have in the camera link application?

    Regards,

    Lee