Part Number: TPD1E05U06-Q1
Other Parts Discussed in Thread: TPD1E05U06, STRIKE, TPD2S300, TPD6S300
Does the TPD1E05U06-Q1 have any benefits over the Central CFTVS5V0BULC BI-DIRECTIONAL TVS
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPD1E05U06-Q1
Other Parts Discussed in Thread: TPD1E05U06, STRIKE, TPD2S300, TPD6S300
Does the TPD1E05U06-Q1 have any benefits over the Central CFTVS5V0BULC BI-DIRECTIONAL TVS
Dear Alec,
Thank so much for that info !
What about the fact that the Central CFTVS5V0BULC is BI-DIRECTIONAL and the TPD1E05U06 is not ?
Best regards
Shmuel
Dear Alec,
I am using these TVS diodes to protect my USB 3.0\3.1 super speed differential signals - thus appears that I should be using a Bi-directional Diode not uni-directional diode no ??????
Best regards
Shmuel
Shmuel-
Sorry for the delay here! Either unidirectional or bidirectional diodes work for USB 3.0/3.1 SS lines because they have differential lines biased around a positive voltage, so it will not drop below zero volts.
The easiest way to get recommendations for ESD devices on an interface is to check our newly released ESD Interface guide which will give the best options for each interface.
Let me know if you have any other questions!
Thanks,
Alec
Dear Alec,
Thanks for the update and the guide. I briefed over it and it was interesting. A couple questions queries :-
1. Since the TPD1E05U06 is uni-directional, doesn't it have the draw back c.f. bi-direction diode that care has to be taken on the polarity of the placement of the part during production ?
2. In the guide it outlines the protection required for Type C solutions. I have placed TPD6S300 (which supposedly takes care of the ESD protection for the USB 2.0 lines and the CC lines) and a TPD2S300 for my 2nd TYPE C connector that has only CC lines connected (which supposedly takes care of the ESD protection for these CC lines). In the guide that you recommended it states that "Device level ESD specifications are not sufficient to protect devices in a system." and "The silicon area required to implement system-level ESD protection is much larger than what is required for device-level". Is it correct that the TPD6S300 \ TPD2S300 provide the system level protection and not the device level protection ? It appears that the TPD6S300 \ TPD2S300 do not provide as much protection as the TPD1E05U06, however do they provide sufficient for my application ?
Best regards
Shmuel