Other Parts Discussed in Thread: BQ25700, TPS65981, TUSB320, TUSB422
Hello;
I am updating a handheld instrument that has a USB type C connector. I am using the USB power to charge the battery. It is safe till 24V - BQ25700.
So,, to make the charging faster, I am looking for the simplest possible solution to tell the PD host to send the most power it can; 15 or 20V, 3A.
Can anybody, please identify a part or solution that, preferrably, is passive - if possible, does not need to communicate with the processor?
The input power goes to a little PCB, that does not have communication lines with the processor. I would prefer not to modify the cabling and the rest of the HW.
Thanks a lot,
Steve