Part Number: TMDSICE3359
Other Parts Discussed in Thread: AM3359, OMAP-L138, TLK110
Hi,
We are designing product using AM3359 and ICEv2.1 board reference.
We are communicating with other 6 OMAP-L138 processor using TL110 and LAN8710A phy ic on backplane mother board.
Longest distance between two devices is 25cm .Each device talking to each other via ethernet swicth of KSZ8999 microcontroller circuit. So we are thinking connection between Phy IC and KSZ8999 should be transformerless.So please can you suggest the blocking capacitor and its value and other precautions should we take. Please suggest the recommended schematics also.
Thanks and Regards,
Ashok Wakode