Part Number: DS125DF1610EVM
Other Parts Discussed in Thread: USB2ANY, DS125DF1610, DPS-DONGLE-EVM
Hello,
I am failing to use the DS125DF1610EVM board with the SigCon Architect software. Following the instructions of the DS125DF1610EVM user's guide, I am stuck at "3. Setup Instructions" at the following step, which I find a bit unclear :
"Using the USB2ANY, the USB cable can be connected directly to the USB port on the EVM board and the computer."
The sentence seems to indicate both that I should use the USB2ANY device and that I can connect the EVM board directly to the computer without using USB2ANY...
Anyway, since I recieved the EVM board without USB2ANY and the SigCon Architect page on TI's website indicates that the DS125DF1610EVM board does not need a dongle since "USB controller is already on-board", I tried to connect directly the EVM board to the computer using the USB A/mini-B cable supplied. Once the board plugged, the D36 LED is on. However, when I open SigCon Architect, I get a pop-up window telling me that "There are no USB2ANY interfaces detected", proposing me to retry or continue in demo mode. In demo mode, when I try to uncheck the "Demo mode" box, the same pop-up window appears. I tried to remove all devices but DS125DF1610 in the devices list and retried the process, for the same results.
I tried to detect the EVM board both before and after enabling my 2.5V power supply connected with banana cables.
Am I doing something wrong?
Thank you in advance,
--
RD