Part Number: SN65HVD232
Other Parts Discussed in Thread: TMS320F28069
Dear TI,
Currently, we use TMS320F28069 to connect as follows.
Problem Phenomenon (Waveform is good when measuring waveform at CPU stage / 120 ohm resistor setting for termination resistance)
1. Communication was established at 1:1.
2. When 1:4 is selected, one of the four motors does not rotate. Not all boards rotate.
3. When it was 1:4, there was and sometimes was not.
-> If the CAN waveform looks normal but it is not communicating, what is the problem?
-> And I checked that the waveforms are coming out well, but I do not have any peaks or noises. How do you determine that the hardware is normal because it seems to be misleading?