Part Number: TPS25820
Other Parts Discussed in Thread: TUSB320, TPS25910
Hi, I have an STM32 that I would like to use with USB-C. I have built a design using the TPS25820 to negotiate and provide power to USB C devices. I plan to use the uc OTG capabilities for USB 2.0 host and device negotiation, and kick on the TPS25820 for any devices detected with no 5V on the USB and maybe gain future proofed downstream capabilities with the TPS25820.
However, when a USB host/downstream port connects on Type C from a Type C (A->C works), no power is sent to the board in device mode. It appears the CC lines on the TPS25820 are interferring (EN is uc controlled so high-z dead or low once powered). Is it EN being high-z when the board is unpowered? How would I work around it if so?
Thanks!