Part Number: LMH0384
Other Parts Discussed in Thread: SD384EVK,
I am using 384EVK kit which SDI cable equalizer. I dont see output coming.
I have Tektronix waveform generator 2300 which is driving cable driver SD303EVK kit and then connected with 75ohm SDI compliance cable and then signal is fed into cable equalizer 3.3V kit and finally signal goes into Tektonix waveform generator.
Problem is when i connect power supply 3.3V to the SDI cable equalizer module i do see on Agilent supply 3.3V set correctly. But as i connect 75 ohm cable to the equalizer kit. Agilent supply read 1.2V not sure why this is happening. It seems when i connect 75ohm cables with BNC connector due to some reason voltage is not stable.
It worked for me for 3 days and then i see this issue and could not resolve.I am thinking this kit could be defective and didn't last long.
Any ideas.