Part Number: TFP403
Other Parts Discussed in Thread: TFP401
Hi Supporter
TFP403 datasheet shows it could support DVI 1.0. Customer need to support HDMI 2.0 and HDMI 1.4. Could you kindly help check if TFP403 could support? Thanks!
Regards
David
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello David,
TFP401 can receive HDMI type digital video signals. HDMI and DVI signals are identical. Note that HDMI 1.3 supports >165MHz pixel clock for extra high resolutions, whereas TFP403 supports <165Mhz.
Regards
Hi Joel
Thanks for confirmation!
So for customer scenario, TPF401 and TFP403, which device is more suitable?
Resolution 1920x1080p@60,pixel clock 148M, HDMI 1.4 and HDMI 2.0.
Regards
David