Part Number: DP83867CR
Dear All,
in the document "Latency in Factory Automation" (snla240) it is written that the user can configure RGMII_TX_HALF_FULL_THR to 0x1 when MAC and PHY share the same clock. It is not completely clear for me which clocks must be the same, because we have at least 3 clocks in the system: RX_CLK (recovered from the network), TX_GTX (supplied by the MAC in the RGZ device) and the PHY local clock at XI pin.
Therefore, my question is: which clocks need to be the same for being able to reduce RGMII_TX_HALF_FULL_THR?
KR,
Tomas