Part Number: SN65HVD96
Hello,
Based on this application note "slla336" we're willing to design power over data communication bus with maximum number of nodes.
Known parameters: +12V DC bus, 20kbps maximum bitrate
Unknown parameters:
- Maximum number of allowed nodes on the same terminated bus
- Maximum number of allowed nodes on an un-terminated bus
The latter application note dos not show the maximum number of nodes; however the datasheet mentions something about 32 and 200 nodes (respectively)
What are the design considerations in order to allow a maximum number of nodes on that specific power over data bus (coil value, capacitors values, etc...)? We have also checked this document "tidu993"
Any support would be much appreciated.