Part Number: DS90UB949-Q1
Other Parts Discussed in Thread: HD3SS3411, HD3SS3411-Q1
I need commutation FPD Link III from two AC-coupled sources such as DS90UB949-Q1. I decided to use HD3SS3411-Q1 for this purpose. This mux/demux has application which described on the page 11, figure 6 in his data sheet. I understand that I have to provide Vbias about 1V for common voltage mode for inputs. Can I use for this purpose usual resistance divider which have HD3SS3411 Evaluation Module? I mean resistors R7-R10 on figure 2 which not installed on this board. Or should I find another solution for this? I'm going to use resistance divider with 220K and 100K.sllu220.pdf