This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS15BR401: No connect pin for replacement DS90LV804

Guru 19685 points

Part Number: DS15BR401
Other Parts Discussed in Thread: DS90LV804, DS15BR400

Please let me confirm about NC pin of DS15BR401;

【Background】

・At first, customer is designing DS90LV804, but they realized that termination resister should put external.

・Most compatible and external termination resister IC is DS15BR401, but below pins are difference.

 DS90LV804 DS15BR401

 1:GND    :N/C

 17:GND   :N/C

 18:GND   :N/C

 19:VDD   :N/C

 22:VDD   :N/C

・Customer is already made circuit board, they can't big change and want not NC pin left open.

【Question】

①Are these NC pin perfectly no connection from internal DS15BR401 circuit? 

②About 19pin and 22pin for DS15BR401, are these pin should connect VDD?

 I think that GND connection is no problem, is it correct?

③Just in case, are 1pin, 17pin, and 18pin connect to GND no problem?

Best regards,

Satoshi

  • Hi Satoshi-san,

    I searched through our DS15BR400/401 documentation and am unable to locate specifics on these pins. Therefore, based on the datasheets alone, I would advise that the pins listed as N/C remain as N/C for proper device operation. I cannot confirm that the device will operate as expected if these N/C pins are connected to VDD or GND.

    May I ask why the device must have external terminations? One thought is that the DS90LV804 can still be used if the customer simply leaves the 100-ohm differential termination resistors unpopulated. Is this an option for your customer?

    Thanks,

    Michael
  • Michael-san

    Thank you for reply,

    About the reason of external termination, customer is using DS15BR401 for multiple line.

    ※Image is below----------------------------------------------------------------------------------------------
    Mother board ←--・・・---Termination resister---→ Multiple board-1
                             |
                              -→Multiple board-2
                            |
    ----------------------------------------------------------------------------------------------------------------------

    Customer should not use internal termination because "double termination".
                             
    One customer update, 19 pin and 22 pin can change NC no problem. (DS90LV804's VDD pin)
    But 1 pin and 17 pin and 18 pin can't change NC by customer's manufacture. (DS90LV804's GND pin)
    If 1 pin and 17 pin and 18 pin can connect GND, this question is clear.

    Best regards,
    Satoshi
  • Hi Satoshi-san,

    The pins are no connect.  They are not connected to anything inside the package.

    Regards,

    Lee