Hi
I have an additional question about the blow posted:
This case is following:
sensnor output: resolution 1280x 720 12 bits , PCLK = 72MHz , Frame format(Line length x Frame length): 2388x 1004 30fps (This is included blanking time.)
use 4 sensors and each one link to UB913 and then to UB964 for one CSI-2 TX port output
And, your answer was:
> 2. I can't understand your issue well. do your camera have sensor and ISP both?
> if input data is 1280x720@30fps with RAW12 bit mode, the total payload rate is
> 331.776Mbps, which is much less than UB964 CSI2's 800Mbps/lane.
> The UB964's CSI2 output rate is fixed by REFCLK freq.
<My question>
Should I need to consider blanking time for CSI-2 throughput in this case?
So, the throughput is 2338 x 1004 x 30fps x 12bit = 845Mbps?
Best Regards
Kenshow