Part Number: DS80PCI102
Hi,
Has the system includedDS80PCI102 passed PCIe 1.1 Compliance Test?
Though my customer is trying to pass PCIe 1.1 Compliance Test, they can not pass below items on their system.
Fail parameter is "Tx, Deemphasized Voltage Ratio".
Output waveform is below;
I think that transition bit should not be implemented deemphasis.
However observed waveform is implemented de-emphasis on transition bit,
Can we delay to implement de-emphasis as red broken line on the above attached file?
or is there any way or confirmation to pass the compliance test?
They use the device as Master mode, I attach writing data.
:10000000000010000004070000ED40000ED4002F97 :10001000AD4002FB1400005F628005F5A8005F5A46 :100020008005F5A800005454FFFFFFFFFFFFFFFF0E :10003000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFD0 :10004000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFC0 :10005000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFB0 :10006000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFA0 :10007000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF90 :10008000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF80 :10009000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF70 :1000A000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF60 :1000B000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF50 :1000C000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF40 :1000D000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF30 :1000E000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF20 :1000F000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF10 :10010000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF :10011000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFEF :10012000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFDF :10013000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFCF :10014000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFBF :10015000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFAF :10016000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF9F :10017000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF8F :10018000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF7F :10019000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF6F :1001A000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF5F :1001B000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF4F :1001C000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF3F :1001D000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF2F :1001E000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF1F :1001F000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF0F :00000001FF
CHA_Sel RATE is set into "1" = GEN1/2 mode.
Please let me know if you have any question.
Best Regards,
Kuramochi