This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DSI85: Stream one DSI video signal to two signle link LVDS displays

Part Number: SN65DSI85

Hello, im a medical devices developer, my plan is to stream same video image to two LVDS displays so I wonder, is it possible to connect single MIPI DSI output from MCU to both DSI inputs A & B of the SN65DSI85 in order to display same image in A & B LVDS outputs (one per display)? 

I know i have to use Dual DSI Inputs (two streams) to two Single-Link LVDS mode but im affraid that if i share same input signals for both inputs A & B the power could not be enough. Im using an STM32F779NI MCU.