Part Number: DP83867E
HI Please we have a few queries;
Issue 1 : No communication established when connected to a 1Gbps capable end device
When using the default Linux and uboot drivers on the board and when the PHY is connected to a PC consisting of 1Gbps capable port, communication failure happens (Board Tx side atleast). The following are further observations.
- On PC side, the Ethernet port is correctly auto negotiated to 100Mbps (since deliberately only 2 pairs of Ethernet on analog side are actually routed on the PCB).
- On the Ti PHY side, I see the auto negotiation result is 100Mbps as well, as expected.
- The auto negotiation advertise settings in the 1000BASE-T Configuration Register (0x09) are populated in the Ti PHY claiming 1Gbps capability (Nothing wrong per say as the PHY is unaware of Analog side routing).
- When I remove 1Gbps advertise capability in the point c above, everything works fine. This removal is infact, provided as a feature in Linux where a device tree node value of “max-speed = <100>” can be provided.
- I have added similar feature in uboot and it works fine too.
- All changes are in the GE github now. I also plan to push this max-speed feature to mainline Xilinx official uboot as well.
Issue 2 : No reply from Ti PHY’s MDIO interface in Linux
The below points summarize this issue
- On PC side, Ethernet interface speed is forced to 100Mbps and then connected to RTM-E board.
- In uboot everything works fine with native drivers.
- In Linux, the DP83867 PHY enters reset with the native Linux DP83867 driver as part of bootup process. The PHY however never recovers and it does not respond on any address 0-31. Most probable cause is software rest using register 0x1f causes issues in this PHY which is how reset is done by this Ti PHY driver.
- This issue is resolved by removing the DP83867 PHY driver and using the generic PHY driver.
Issue 3 : Strange PHY address
Refer to my in email for information;
Can you advice best help??
thanks Linda