Part Number: TLK106L
Other Parts Discussed in Thread: DP83822I, TLK105L
Hi!
We have an issue with the ethernet communication over the TLK106L.
Our System works in normal operation. We cyclically ping the TLK106L. If we turn the ETH-Link off and on, it starts that we lost about 7%-10% of the pings. This can even happen sometimes, if we do not switch the link. While researching the problem, we consider the TX Signal of the ETH PHY. If we measure the RX and TX signal from the TLK106L, we can see a strange waveform on the TX signal. You can see the waveform in the attached file. The TX signal from the TLK106L shows a rippelvoltage with about 1GHz. Have anybody else seen this waveform with a TLK106L? Is this a known issue of the TLK106L, or an normal behavoir?
You can see that the Rippel is damped by the ETH Cabel. If we increase the length of the cabel, the signals gets even better, but this is expected.
Best regards
Kevin