Other Parts Discussed in Thread: DS90UB926Q-Q1, DS90UB940-Q1, DS90UB928Q-Q1, , DS90UB948-Q1
so if you look on the TI table for the DS90UB947 SER, it shows the preferred (recommended) DES is the '948. How tightly is this coupling?
could you use the DES DS90UB926?
It seems the reason TI specifies a single pair (947/948) is the assumption that the input to the SER is going to be the output to the DES. However, there are cases where you might want an LVTTL input and an R/G/B/PCLK output to save not using a conversion chip.
Please note I am assuming the protocol between mismatched pairs are always going to be incompatible. Otherwise TI would show multiple pairings. This is more a paranoia check...
I assume this is a question for TI tech support...