Hi Team,
VIH and VIL of electrical characteristics shows the following.
Should we consider the max value of VIH (VIN) and min value of VIL (GND) is mandatory?
I believe there could be the case that overshoot (undershoot) is occured and exceed more than VIN (less than GND) instantaneously.
note) I understood absolute maximum rating -0.3~(VDDIO+0.3)[V] should be satisfied in this case.
Best Regards,
Yaita / Japan disty