Part Number: DP83822IF
Hi all
Would you mind if we ask DP83822IF?
We would like to confirm the operation of PHY Software Reset (B15=1, Address 0x0000).
<Question1>
How long does it rquire that PHY returns to default condition?
Is it the same as hardware reset(7.7 Timing Requirements, Reset Timing on the datasheet P11)?
About MDC communicatio, does it require 195ms(T2 : Post power-up stabilization time prior to MDC preamble for register accesses) after software reset?
There is the description "This bit is self cleared and has the same effect as Hardware reset pin." on 0x001F.
However, we could not judge it.
<Question2>
After software reset, will the register data of 0x0017(RMII and Status Register (RCSR)) return to default condition?
Kind regards,
Hirotaka Matsumoto