Part Number: DS90UB913A-Q1
Other Parts Discussed in Thread: DS90UB914A-CXEVM
Tool/software: Linux
Hello,
DS90UB913A and 914 are used in our camera design. And 5M cable is used to connect these two chips. The camera works OK. But the image is disordered during the EFT(Electrical Fast Transient) Test when it goes up to 500V. In fact, it needs to pass 2KV in the application. The case of camera and receiver is metal and is connected to GND. So the whole system has one GND. We believe the shielding is fine.
Do we need to add some common mode filter on the signal? If so how to add that?
Does anyone have idea on this issue?
Thanks,
Bob