Other Parts Discussed in Thread: DS90UB954-Q1
The DS90UB954-Q1 has a register setting, "BC_FREQ_SELECT" bits of the BCC_CONFIG register, that can change the back-channel frequency to 25 Mbps instead of the default 50 Mbps in Synchronous mode. Is this setting usable with the DS90UB953-Q1 serializer? I did not find an equivalent setting in the register set for the DS90UB953-Q1. However in the data sheet I found in paragraph 7.3.3:
"The back channel frequency is programmable for operation with compatible deserializers."
Other than the MODE setting, I don't see a way to program the back channel frequency.