Part Number: TPS2553D
Hi,
I have a question on TPS2553DDBVR Operating Junction Temperature.
Under Item 7.3 Recommended Operating Conditions spec, Tj max is 105degC for Iout=1.5A.
Under item 7.5 Electrical Characteristic, Thermal shutdown will occur at 135degC.
May I know what are the differences between these two items spec?
Does it mean for Iout=1.5A, the junction temperature measured/calculated cannot exceed 105degC?
What would happen to the device if Tj is more than 105degC? Operation will be disabled? And any tolerance of 105+- ?degC if the device hits max Tj before it disabled?
And per understanding, thermal shutdown will only occur at 135degC, right?
Please do kindly help to advise, thanks.
Best Regards,
Philip