Part Number: DS90UB954-Q1
Hi,
I am using the Sony IMX274 connected to the DS90UB953 serializer to the DS90UB954 de-serializer. The sensor setup works normally, when not passing through the FPD3-LINK, but with the DS90UB953/4 pair I get a thin strip of valid image data (about 192 pixels) with the rest of the line being corrupted.
I am not getting any CSI errors (registers 0x5c-0x60 are 0), and 0x61 consistently reports 0x12
It looks like the imager frame output looks like this:
[HDR: 0x00, Frame Start]
[HDR: 0x12, Embedded data (140 bytes+46 pad bytes), PF]
[HDR: 0x37, Black Pixels, PF]
[HDR: RAW12 0x2c, Image Data (1920 pixels), PF]
. . .
1080 lines total
. . .
[HDR: RAW12, Image Data, PF]
[HDR: 0x01, Frame End]
The image output looks like this:
Any idea why the lines would be truncated like this?
Thanks,
Adam