Other Parts Discussed in Thread: TPS25741, TPS65981
We are developing a USB-C Host and a USB-C Device electronic which shall use USB PD to provide 24V/3A. We're using TI TPS25741 as USB PD source controller. It is configured to be able to deliver 24V/3A after PD communication with the device. Now we need a "companion" chip for the USB device. In best case it should be a standalone ic which shows the USB host that it wants 24V/3A. We would then have a 24V power supply for our device electronic which starts operation after 24V is applied by the USB host (TPS25741).