Part Number: TPD2S300
Hi,
My customer has the following questions:
It looks like the GND pin is buried in the center ball of the package. Thus, it cannot be routed out using conventional "drill" vias on a PCB. Their concern is only micro laser vias can be used which will add complexity to manufacturing process, unless they tie the FLT# line to GND as well to make a path for Ground to connect.
Two questions:
1. Do have you an alternate package that uses a larger package or alternate pin-out? - does not look like other packages are available
2. If we choose not to use the FLT# pin, can I tie this pin to GND? My understanding is that FLT# will either be Hi-Z (no fault) or tied to GND (LOW) during a fault condition. Is ther an internal pullup on this pin?
Thanks,
Chuchen