Part Number: DS90UB921-Q1EVM
Other Parts Discussed in Thread: DS90UB921-Q1, ALP, DS90UB926QSEVB
I'm trying to evaluate a SerDes pair of DS90UB921-Q1 and DS90UB926Q for our future use with their respective evaluation kits.
When I start the ALP software, it does inform me on the bottom line that "Hardware Connected". However, even after disabling demo mode and manually changing the device from DS90UH925 to UB921, the detailed device information tab (opened by clicking the device from the list on the left) shows the wrong device UH925.
Moreover, ALP keeps freezing periodically so badly that it is almost impossible even to open the above mentioned tab. This only happens after I try to connect the DS90UB921, if I keep it disconnected ALP seems to work just fine.
Reading I2C registers from the 'Registers" tab seems like ALP is trying to do something, but all registers have value 0. Which is not surprising, since ALP is probably trying to read from a device that is not actually connected (the UH925).
ALP version is 1.56.0010
I've been using
as my guide, and the EVM is showing in Windows Device Manager as "HID-compliant device" as mentioned there, so it seems that the setup itself should be correct.