Other Parts Discussed in Thread: SN74LV08A
Hello,
this is my very first question.
Referring to the RS-485 Bidirectional Fan-Out Hub With Automatic Direction Control Reference Design, I would like to know why the R outputs of the 4 RS-485 transceivers are connected to the T input od the single RS-485 transceiver through the SN74LV08A and not directly. I mean, why the 4 R outputs are not connected together and directly connected ti the T input of the left transceiver?
I need to make an RS-485 bidirectional splitter (1 to N) with automatic direction control.
Thank you very much for the support.
Roberto