Part Number: TUSB4041I
Dear To Whom it Might Concern,
I ask this question on behalf of another engineer who intend to use the TUSB4041I. There is one thing in the data sheet that bewilders us: p.14 - 8.3.7 Power-Up and Reset.
"The TUSB4041I device does not have specific power-sequencing requirements with respect to the core power
(VDD) or I/O and analog power (VDD33). The core power (VDD) or I/O power (VDD33) can be powered up for an
indefinite period of time while the other is not powered up if all of the following constraints are met:
• Observe all maximum ratings and recommended operating conditions.
• Observe all warnings about exposure to maximum rated and recommended conditions, particularly junction
temperature. These apply to power transitions and normal operation.
• Limit bus contention to 100 hours over the projected lifetime of the device while VDD33 is powered-up.
• Do not exceed the ratings listed in the Absolute Maximum Ratings table for bus contention while VDD33 is
powered-down."
In regards to the thirds bullet, what does this sentence signify? What happens after 100hrs?
Thanks in advance,
Gustaf Falk Olson