Part Number: TPD4E001
Hello,
Our customer using TPD4E001DRLR, sometimes failure occur in the end customers.
This device is passed IEC61000-4-2 and 4-5, so they think the cause for failure seems that a burst(61000-4-4) noise had injected
or some continuous excessive current had injected.
Therefore, they want to know the absolute maximum ratings of continuous current for each diode inside the device.
(in almost all discrete ESD protection diode, that value is shown in the datasheet. so they think TPD device can also show it)
Could you show these values ?
Thanks and best regards,
Hiro