Part Number: TLK10232
Other Parts Discussed in Thread: DS125DF1610
Does TLK10232 can run at 1.25G general purpose mode. I need it to bypass all 1000-x signal. does it OK?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TLK10232
Other Parts Discussed in Thread: DS125DF1610
Does TLK10232 can run at 1.25G general purpose mode. I need it to bypass all 1000-x signal. does it OK?
Thanks
I use it with reference clock 312.5Mhz.
MPY=8 both HS and LS
LS Q rate HS Eight rate
01 -->3402
I connect it to DS125DF1610, it will have error. when it use at KR mode, it is OK. But, I need it as repeater only.
my design
sfp --> ds125df160 --> tlk10232 --> 1G phy.
when I work at general purpose mode 1.25G with 312.5Mhz, reg 0x10 = 0 and reg 0x0f = 0x1E1B.
does it need to care bit "4"?
7 TX_FIFO_UNDERFLOW Not applicable in 1GKX mode. When high, indicates underflow has occurred in RO/LH
(RG) the transmit datapath (CTC) FIFO.
6 TX_FIFO_OVERFLOW When high, in 10GKR and 10G modes indicates overflow has occurred in the RO/LH
(RXG) transmit datapath (CTC) FIFO.
5 RX_FIFO_UNDERFLOW Not applicable in 1GKX mode. When high, indicates underflow has occurred in RO/LH
(RG) the receive datapath (CTC) FIFO.
4 RX_FIFO_OVERFLOW In 10GKR and 10G modes, high indicates overflow has occurred in the receive RO/LH
(RXG) datapath (CTC) FIFO. In 1G-KX mode, high indicates a FIFO error.
Hi Cannie,
Could you try the next procedure?
General Purpose Mode 1:1
REFCLK: 153.6/122.88MHz
1. Ensure ST input pin is Low.
2. Ensure MODE_SEL input pin is High.
3. Ensure PRBSEN input pin is Low.
4. Ensure REFCLK_SEL pin is Low.
5. Reset device (Issue a hard reset or soft reset, RESET_N asserted for at least 10us or write 1b'1 to 30.0.15
6. Write 4'b1011/1101 to 30.2.3:0 to set HS_PLL_MULt multiplier to 16/20x
7. Write 2'b01 to 30.3.9:8 to set HS_RATE_TX to Eight Rate.
8. Write 3'b101 to 30.3.2:0 to set HS_RATE_RX to Eight Rate.
9. Write 2'b11 to 30.1.13:12 to set mode 1:1
10. Write 2'b01 to 30.7.9:8 to set LS TX SerDes lane rate to Half Rate.
11. Write 2'b01 to 30.7.1:0 to set LS RX SerDes lane rate to Half Rate.
12. Issue a data path reset. Write 1'b1 to 30.14.3
13. Wait for 1000ms.
Please try the procedure above and let us know your results.
Best Regards,
Luis Omar Moran
High Speed Interface
SWAT Team