Part Number: DP83867IS
Dear TI support, colleagues,
our problem/goal seems to be equivalent as described in the following thread on this forum:
https://e2e.ti.com/support/interface/ethernet/f/903/p/584209/2149151
but that thread is locked and no solution is described there, so, please, let me describe the problem in my own words.
Intended result
We need the best possible link-up time after cable (CAT5E) connection is established between two our custom boards equipped with DP83867IS. We would like to reach link-up times around 10ms if possible, less then 30ms is still usable. To reach this time with 1000BASE-T, the auto-negotiation and auto-crossing can be disabled and master and slave can be set manually, this is perfectly acceptable solution for us.
So the signal chain is:
MAC <--- SGMII ---> DP83867IS <--- CAT5E crossover cable ---> DP83867IS <--- SGMII ---> MAC
Success with 100BASE-TX
With 100BASE-TX fixed mode and manual MDI configuration with crossover cable we reached quite fast (10ms with short cable, 43ms with 130 meters long cable) link-up time. We used following settings:
- Set manual MDI configuration: PHY Control Register (PHYCR), address 0x0010 <- 0x5808
- Set 100Mpbs speed and full duplex: Basic Mode Control Register (BMCR), address 0x0000 <- 0x2100
Failure with 1000BASE-T
With 1000BASE-T fixed mode, manual MDI configuration and setting one DP83867IS to master and second DP83867IS to slave the link never comes up (both DP83867ISs report link down regardless of CAT5e cable connection). We used following settings:
- Set manual MDI configuration: PHY Control Register (PHYCR), address 0x0010 <- 0x5808
- Set 1000Mpbs speed and full duplex: Basic Mode Control Register (BMCR), address 0x0000 <- 0x0140
- Set manual master/slave configuration: Configuration Register 1 (CFG1), address 0x0009
- Set manual master configuration in the first DP83867IS: CFG1 <- 0x1F00
- Set manual slave configuration in the second DP83867IS: CFG1 <- 0x1300
Register dump
I attach complete DP83867IS register dump. First DP83867IS has MDIO address 6, second DP83867IS has MDIO address 7. There are three different scenarios in the table:
- Default power-on configuration (auto-negotiation enabled): After cable was connected, 1000BASE-T link was established and the dump was made on both PHYs.
- Fixed 100BASE-TX (auto-negotiation disabled): After cable was connected, 100BASE-TX link was established and the dump was made on both PHYs.
- Fixed 1000BASE-T (auto-negotiation disabled): After cable was connected, no link was established and the dump was made after five seconds.
The relevant fields with changes we made after power on configuration:
| register address | PHY6: default | PHY7: default | PHY6: 100BASE-TX | PHY7: 100BASE-TX | PHY6: 1000BASE-T Master | PHY7: 1000BASE-T Slave |
| 0x0000 |
0x1140 |
0x1140 | 0x2100 | 0x2100 | 0x0140 | 0x0140 |
| 0x0001 | 0x796D | 0x796D | 0x794D | 0x794D | 0x7949 | 0x7949 |
| 0x0009 | 0x0300 | 0x0300 | 0x0300 | 0x0300 | 0x1F00 | 0x1300 |
| 0x0010 | 0x5848 | 0x5848 | 0x5808 | 0x5808 | 0x5808 | 0x5808 |
Complete register dump (CSV file):
Register address,PHY6: default,PHY7: default,PHY6: 100BASE-TX,PHY7: 100BASE-TX,PHY6: 1000BASE-T Master,PHY7: 1000BASE-T Slave 0x0000, 0x1140, 0x1140, 0x2100, 0x2100, 0x0140, 0x0140 0x0001, 0x796D, 0x796D, 0x794D, 0x794D, 0x7949, 0x7949 0x0002, 0x2000, 0x2000, 0x2000, 0x2000, 0x2000, 0x2000 0x0003, 0xA231, 0xA231, 0xA231, 0xA231, 0xA231, 0xA231 0x0004, 0x01E1, 0x01E1, 0x01E1, 0x01E1, 0x01E1, 0x01E1 0x0005, 0xC1E1, 0xC1E1, 0x0000, 0x0000, 0x0000, 0x0000 0x0006, 0x006F, 0x006F, 0x0064, 0x0064, 0x0064, 0x0064 0x0007, 0x2001, 0x2001, 0x2001, 0x2001, 0x2001, 0x2001 0x0008, 0x4800, 0x4800, 0x0000, 0x0000, 0x0000, 0x0000 0x0009, 0x0300, 0x0300, 0x0300, 0x0300, 0x1F00, 0x1300 0x000A, 0x7C00, 0x3C00, 0x0000, 0x0000, 0x0000, 0x0000 0x000B, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x000C, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x000D, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x000E, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x000F, 0x3000, 0x3000, 0x3000, 0x3000, 0x3000, 0x3000 0x0010, 0x5848, 0x5848, 0x5808, 0x5808, 0x5808, 0x5808 0x0011, 0xBC02, 0xBC02, 0x6C02, 0x6C02, 0xA802, 0xA802 0x0012, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0013, 0x1C44, 0x1C44, 0x0444, 0x0444, 0x0044, 0x0044 0x0014, 0x29C7, 0x29C7, 0x29C7, 0x29C7, 0x29C7, 0x29C7 0x0015, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0016, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0017, 0x0040, 0x0040, 0x0040, 0x0040, 0x0040, 0x0040 0x0018, 0x6150, 0x6150, 0x6150, 0x6150, 0x6150, 0x6150 0x0019, 0x4444, 0x4444, 0x4444, 0x4444, 0x4444, 0x4444 0x001A, 0x0002, 0x0002, 0x0002, 0x0002, 0x0002, 0x0002 0x001B, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x001C, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x001D, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x001E, 0x0002, 0x0002, 0x0002, 0x0002, 0x0002, 0x0002 0x001F, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0020, 0x5668, 0x5668, 0x5668, 0x5668, 0x5668, 0x5668 0x0021, 0x5814, 0x5814, 0x5814, 0x5814, 0x5814, 0x5814 0x0022, 0x0718, 0x0718, 0x0718, 0x0718, 0x0718, 0x0718 0x0023, 0x8D1C, 0x8D1C, 0x8D1C, 0x8D1C, 0x8D1C, 0x8D1C 0x0024, 0xF01E, 0xF01E, 0xF01E, 0xF01E, 0xF01E, 0xF01E 0x0025, 0x0400, 0x0400, 0x0400, 0x0400, 0x0400, 0x0400 0x0026, 0x008D, 0x008D, 0x008D, 0x008D, 0x008D, 0x008D 0x0027, 0xF810, 0xF810, 0xF810, 0xF810, 0xF810, 0xF810 0x0028, 0xFF80, 0xFF80, 0xFF80, 0xFF80, 0xFF80, 0xFF80 0x0029, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x002A, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x002B, 0x0100, 0x0100, 0x0100, 0x0100, 0x0100, 0x0100 0x002C, 0x141F, 0x141F, 0x141F, 0x141F, 0x141F, 0x141F 0x002D, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x002E, 0x0221, 0x0221, 0x0221, 0x0221, 0x0221, 0x0221 0x002F, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0030, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0031, 0x10B0, 0x10B0, 0x10B0, 0x10B0, 0x10B0, 0x10B0 0x0032, 0x00D3, 0x00D3, 0x00D3, 0x00D3, 0x00D3, 0x00D3 0x0033, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0034, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0035, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0036, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0037, 0x0003, 0x0003, 0x0003, 0x0003, 0x0003, 0x0003 0x0038, 0x0001, 0x0001, 0x0001, 0x0001, 0x0001, 0x0001 0x0039, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x003A, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x003B, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x003C, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x003D, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x003E, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x003F, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0040, 0x0073, 0x0073, 0x0073, 0x0073, 0x0073, 0x0073 0x0041, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0042, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0043, 0x07A0, 0x07A0, 0x07A0, 0x07A0, 0x07A0, 0x07A0 0x0044, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0045, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0046, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0047, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0048, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0049, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x004A, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x004B, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x004C, 0x1E00, 0x1E00, 0x0200, 0x0200, 0x0800, 0x1000 0x004D, 0x0055, 0x0055, 0x0001, 0x0001, 0x0055, 0x0055 0x004E, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x004F, 0x0136, 0x0116, 0x0166, 0x0146, 0x0196, 0x0146 0x0050, 0x0453, 0x0453, 0x0453, 0x0453, 0x0453, 0x0453 0x0051, 0x9ADA, 0x9ADA, 0x9ADA, 0x9ADA, 0x9ADA, 0x9ADA 0x0052, 0x01F4, 0x01F4, 0x01F4, 0x01F4, 0x01F4, 0x01F4 0x0053, 0x2055, 0x2055, 0x2055, 0x2055, 0x2055, 0x2055 0x0054, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0055, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0056, 0x0020, 0x0060, 0x0020, 0x0060, 0x0060, 0x0060 0x0057, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0058, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0059, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x005A, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x005B, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x005C, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x005D, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x005E, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x005F, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0060, 0x0008, 0x0008, 0x0008, 0x0008, 0x0008, 0x0008 0x0061, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0062, 0x0001, 0x0001, 0x0001, 0x0001, 0x0001, 0x0001 0x0063, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0064, 0x8000, 0x8000, 0x8000, 0x8000, 0x8000, 0x8000 0x0065, 0x43AA, 0x43AA, 0x43AA, 0x43AA, 0x43AA, 0x43AA 0x0066, 0x2334, 0x2334, 0x2334, 0x2334, 0x2334, 0x2334 0x0067, 0x03E8, 0x03E8, 0x03E8, 0x03E8, 0x03E8, 0x03E8 0x0068, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0069, 0x0020, 0x0020, 0x0020, 0x0020, 0x0020, 0x0020 0x006A, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x006B, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x006C, 0x0289, 0x0289, 0x0289, 0x0289, 0x0289, 0x0289 0x006D, 0x8912, 0x8912, 0x8912, 0x8912, 0x8912, 0x8912 0x006E, 0x0806, 0x0807, 0x0806, 0x0807, 0x0806, 0x0807 0x006F, 0x0100, 0x0100, 0x0100, 0x0100, 0x0100, 0x0100 0x0070, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0071, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0072, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0073, 0x0600, 0x0600, 0x0000, 0x0000, 0x0000, 0x0000 0x0074, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0075, 0x00C0, 0x00C0, 0x0000, 0x0000, 0x0000, 0x0000 0x0076, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0077, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0078, 0x05ED, 0x05ED, 0x05ED, 0x05ED, 0x05ED, 0x05ED 0x0079, 0x003F, 0x003F, 0x003F, 0x003F, 0x003F, 0x003F 0x007A, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x007B, 0x05DC, 0x05DC, 0x05DC, 0x05DC, 0x05DC, 0x05DC 0x007C, 0x007D, 0x007D, 0x007D, 0x007D, 0x007D, 0x007D 0x007D, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x007E, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x007F, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0080, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0081, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0082, 0x5AD6, 0x5695, 0x5AD6, 0x5695, 0x5AD6, 0x5695 0x0083, 0x7FF6, 0x7FF5, 0x03F6, 0x03F5, 0x7FF6, 0x7FF5 0x0084, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0085, 0x007E, 0x007E, 0x007E, 0x007E, 0x007E, 0x007E 0x0086, 0x0077, 0x0077, 0x0077, 0x0077, 0x0077, 0x0077 0x0087, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0088, 0x03FF, 0x03FF, 0x03FF, 0x03FF, 0x03FF, 0x03FF 0x0089, 0x8000, 0x8000, 0x8000, 0x8000, 0x8000, 0x8000 0x008A, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x008B, 0x0BBB, 0x0AAA, 0x0BBB, 0x0AAA, 0x0BBB, 0x0AAA 0x008C, 0x9999, 0x9999, 0x9999, 0x9999, 0x9999, 0x9999 0x008D, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x008E, 0x0010, 0x0010, 0x0010, 0x0010, 0x0010, 0x0010 0x008F, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0090, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0091, 0x0210, 0x0210, 0x0210, 0x0210, 0x0210, 0x0210 0x0092, 0x0210, 0x0210, 0x0210, 0x0210, 0x0210, 0x0210 0x0093, 0xBBBB, 0xBBBB, 0xBBBB, 0xBBBB, 0xBBBB, 0xBBBB 0x0094, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0095, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0096, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0097, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0098, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0099, 0x4000, 0x4000, 0x4000, 0x4000, 0x4000, 0x4000 0x009A, 0x0285, 0x0285, 0x0285, 0x0285, 0x0285, 0x0285 0x009B, 0x0285, 0x0285, 0x0285, 0x0285, 0x0285, 0x0285 0x009C, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x009D, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x009E, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x009F, 0xBBBB, 0xBBBB, 0xBBBB, 0xBBBB, 0xBBBB, 0xBBBB 0x00A0, 0x0707, 0x0507, 0x0707, 0x0507, 0x0707, 0x0507 0x00A1, 0x0807, 0x0908, 0x0807, 0x0908, 0x0807, 0x0908 0x00A2, 0x1010, 0x1010, 0x1010, 0x1010, 0x1010, 0x1010 0x00A3, 0x1010, 0x1010, 0x1010, 0x1010, 0x1010, 0x1010 0x00A4, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x00A5, 0x8888, 0x8888, 0x8888, 0x8888, 0x8888, 0x8888 0x00A6, 0x0783, 0x0803, 0x0783, 0x0803, 0x0783, 0x0803 0x00A7, 0xFFFF, 0xFFFF, 0xFFFF, 0xFFFF, 0xFFFF, 0xFFFF 0x00A8, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x00A9, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x00AA, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x00AB, 0x3543, 0x4243, 0x9834, 0xB854, 0x4444, 0x4444 0x00AC, 0x2403, 0x4544, 0x5554, 0x7744, 0x4444, 0x4444 0x00AD, 0x012A, 0x0169, 0x00E9, 0x0169, 0x00E9, 0x00E7 0x00AE, 0x0126, 0x00A9, 0x01F2, 0x0273, 0x00ED, 0x010B 0x00AF, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x00B0, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x00B1, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x00B2, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x00B3, 0x0088, 0x0088, 0x0088, 0x0088, 0x0088, 0x0088 0x00B4, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x00B5, 0x1020, 0x1020, 0x1020, 0x1020, 0x1020, 0x1020 0x00B6, 0x1020, 0x1020, 0x1020, 0x1020, 0x1020, 0x1020 0x00B7, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x00B8, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x00B9, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x00BA, 0x7777, 0x7777, 0x7777, 0x7777, 0x7777, 0x7777 0x00BB, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x00BC, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x00BD, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x00BE, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x00BF, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x00C0, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x00C1, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x00C2, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x00C3, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x00C4, 0x1F1F, 0x1F1F, 0x1F1F, 0x1F1F, 0x1F1F, 0x1F1F 0x00C5, 0x0003, 0x0003, 0x0003, 0x0003, 0x0003, 0x0003 0x00C6, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x00C7, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x00C8, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x00C9, 0x7000, 0x7000, 0x7000, 0x7000, 0x7000, 0x7000 0x00CA, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x00CB, 0x00C1, 0x0F7E, 0x00C1, 0x0F7E, 0x00C1, 0x0F7E 0x00CC, 0x2600, 0x2500, 0x2600, 0x2500, 0x2600, 0x2500 0x00CD, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x00CE, 0xFC00, 0xFC00, 0xFC00, 0xFC00, 0xFC00, 0xFC00 0x00CF, 0x0300, 0x3D00, 0x0300, 0x3D00, 0x0300, 0x3D00 0x00D0, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x00D1, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x00D2, 0x0002, 0x0002, 0x0002, 0x0002, 0x0002, 0x0002 0x00D3, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x00D4, 0x0F00, 0x1000, 0x0F00, 0x1000, 0x0F00, 0x1000 0x00D5, 0xC390, 0xC390, 0xC390, 0xC390, 0xC390, 0xC390 0x00D6, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x00D7, 0x0300, 0x0300, 0x0100, 0x0300, 0x0200, 0x0200 0x00D8, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x00D9, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x00DA, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x00DB, 0x0010, 0x0010, 0x0010, 0x0010, 0x0010, 0x0010 0x00DC, 0x3800, 0x3800, 0x3800, 0x3800, 0x3800, 0x3800 0x00DD, 0x0200, 0x0200, 0x0200, 0x0200, 0x0200, 0x0200 0x00DE, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x00DF, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x00E0, 0x3220, 0x3220, 0x3220, 0x3220, 0x3220, 0x3220 0x00E1, 0x30C0, 0x30C0, 0x30C0, 0x30C0, 0x30C0, 0x30C0 0x00E2, 0x7A56, 0x7A56, 0x7A56, 0x7A56, 0x7A56, 0x7A56 0x00E3, 0x204B, 0x204B, 0x204B, 0x204B, 0x204B, 0x204B 0x00E4, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x00E5, 0x0231, 0x0231, 0x0231, 0x0231, 0x0231, 0x0231 0x00E6, 0x0231, 0x0231, 0x0231, 0x0231, 0x0231, 0x0231 0x00E7, 0x0C83, 0x0C83, 0x0C83, 0x0C83, 0x0C83, 0x0C83 0x00E8, 0x9696, 0x9696, 0x9696, 0x9696, 0x9696, 0x9696 0x00E9, 0x9F22, 0x9F22, 0x9F22, 0x9F22, 0x9F22, 0x9F22 0x00EA, 0x2040, 0x2040, 0x2040, 0x2040, 0x2040, 0x2040 0x00EB, 0x0501, 0x0501, 0x0501, 0x0501, 0x0501, 0x0501 0x00EC, 0x190D, 0x190D, 0x190D, 0x190D, 0x190D, 0x190D 0x00ED, 0x6432, 0x6432, 0x6432, 0x6432, 0x6432, 0x6432 0x00EE, 0xFA96, 0xFA96, 0xFA96, 0xFA96, 0xFA96, 0xFA96 0x00EF, 0x1840, 0x1840, 0x1840, 0x1840, 0x1840, 0x1840 0x00F0, 0x3E25, 0x3E25, 0x3E25, 0x3E25, 0x3E25, 0x3E25 0x00F1, 0x6004, 0x6004, 0x6004, 0x6004, 0x6004, 0x6004 0x00F2, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x00F3, 0x0040, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x00F4, 0x6791, 0x6791, 0x6791, 0x6791, 0x6791, 0x6791 0x00F5, 0x199A, 0x199A, 0x199A, 0x199A, 0x199A, 0x199A 0x00F6, 0x1027, 0x1027, 0x1027, 0x1027, 0x1027, 0x1027 0x00F7, 0x051C, 0x051C, 0x051C, 0x051C, 0x051C, 0x051C 0x00F8, 0x1027, 0x1027, 0x1027, 0x1027, 0x1027, 0x1027 0x00F9, 0xAC76, 0xAC76, 0xAC76, 0xAC76, 0xAC76, 0xAC76 0x00FA, 0x3033, 0x3033, 0x3033, 0x3033, 0x3033, 0x3033 0x00FB, 0x3104, 0x3104, 0x3104, 0x3104, 0x3104, 0x3104 0x00FC, 0x0067, 0x0067, 0x0067, 0x0067, 0x0067, 0x0067 0x00FD, 0x199A, 0x199A, 0x199A, 0x199A, 0x199A, 0x199A 0x00FE, 0xE721, 0xE721, 0xE721, 0xE721, 0xE721, 0xE721 0x00FF, 0x1027, 0x1027, 0x1027, 0x1027, 0x1027, 0x1027 0x0100, 0x051C, 0x051C, 0x051C, 0x051C, 0x051C, 0x051C 0x0101, 0x1027, 0x1027, 0x1027, 0x1027, 0x1027, 0x1027 0x0102, 0x6333, 0x6333, 0x6333, 0x6333, 0x6333, 0x6333 0x0103, 0x4454, 0x4454, 0x4454, 0x4454, 0x4454, 0x4454 0x0104, 0x2447, 0x2447, 0x2447, 0x2447, 0x2447, 0x2447 0x0105, 0x0012, 0x0012, 0x0012, 0x0012, 0x0012, 0x0012 0x0106, 0x7A56, 0x7A56, 0x7A56, 0x7A56, 0x7A56, 0x7A56 0x0107, 0x64FF, 0x64FF, 0x64FF, 0x64FF, 0x64FF, 0x64FF 0x0108, 0x00A4, 0x00A4, 0x00A4, 0x00A4, 0x00A4, 0x00A4 0x0109, 0x00AA, 0x00AA, 0x00AA, 0x00AA, 0x00AA, 0x00AA 0x010A, 0x00FE, 0x00FE, 0x00FE, 0x00FE, 0x00FE, 0x00FE 0x010B, 0x0500, 0x0500, 0x0500, 0x0500, 0x0500, 0x0500 0x010C, 0x7776, 0x7776, 0x7776, 0x7776, 0x7776, 0x7776 0x010D, 0x00FC, 0x00FC, 0x00FC, 0x00FC, 0x00FC, 0x00FC 0x010E, 0x00EE, 0x00EE, 0x00EE, 0x00EE, 0x00EE, 0x00EE 0x010F, 0x6752, 0x6752, 0x6752, 0x6752, 0x6752, 0x6752 0x0110, 0x6143, 0x6143, 0x6143, 0x6143, 0x6143, 0x6143 0x0111, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0112, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0113, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0114, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0115, 0xB8BB, 0xB8BB, 0xB8BB, 0xB8BB, 0xB8BB, 0xB8BB 0x0116, 0xDDCC, 0xDDCC, 0xDDCC, 0xDDCC, 0xDDCC, 0xDDCC 0x0117, 0xAABD, 0xAABD, 0xAABD, 0xAABD, 0xAABD, 0xAABD 0x0118, 0x8BF9, 0x8BF9, 0x8BF9, 0x8BF9, 0x8BF9, 0x8BF9 0x0119, 0xFFA4, 0xFFA4, 0xFFA4, 0xFFA4, 0xFFA4, 0xFFA4 0x011A, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x011B, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x011C, 0xFCFC, 0xFCFC, 0xFCFC, 0xFCFC, 0xFCFC, 0xFCFC 0x011D, 0x6B6A, 0x6B6A, 0x6B6A, 0x6B6A, 0x6B6A, 0x6B6A 0x011E, 0x2FF8, 0x2FF8, 0x2FF8, 0x2FF8, 0x2FF8, 0x2FF8 0x011F, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0120, 0x00CE, 0x00CE, 0x00CE, 0x00CE, 0x00CE, 0x00CE 0x0121, 0x0099, 0x0099, 0x0099, 0x0099, 0x0099, 0x0099 0x0122, 0x0D14, 0x0D14, 0x0D14, 0x0D14, 0x0D14, 0x0D14 0x0123, 0x006D, 0x006D, 0x006D, 0x006D, 0x006D, 0x006D 0x0124, 0x0404, 0x0404, 0x0404, 0x0404, 0x0404, 0x0404 0x0125, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0126, 0x0010, 0x0010, 0x0010, 0x0010, 0x0010, 0x0010 0x0127, 0x0202, 0x0202, 0x0202, 0x0202, 0x0202, 0x0202 0x0128, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0129, 0x0002, 0x0002, 0x0002, 0x0002, 0x0002, 0x0002 0x012A, 0xFFFF, 0xFFFF, 0xFFFF, 0xFFFF, 0xFFFF, 0xFFFF 0x012B, 0xA690, 0xA690, 0xA690, 0xA690, 0xA690, 0xA690 0x012C, 0x0C2D, 0x0C2D, 0x0C2D, 0x0C2D, 0x0C2D, 0x0C2D 0x012D, 0x0009, 0x0009, 0x0009, 0x0009, 0x0009, 0x0009 0x012E, 0x8AC8, 0x8AC8, 0x8AC8, 0x8AC8, 0x8AC8, 0x8AC8 0x012F, 0x7520, 0x7520, 0x7520, 0x7520, 0x7520, 0x7520 0x0130, 0x0200, 0x0200, 0x0200, 0x0200, 0x0200, 0x0200 0x0131, 0x4A23, 0x4A23, 0x4A23, 0x4A23, 0x4A23, 0x4A23 0x0132, 0x6520, 0x6520, 0x6520, 0x6520, 0x6520, 0x6520 0x0133, 0x4820, 0x4820, 0x4820, 0x4820, 0x4820, 0x4820 0x0134, 0x1000, 0x1000, 0x1000, 0x1000, 0x1000, 0x1000 0x0135, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0136, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0137, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0138, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0139, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x013A, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x013B, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x013C, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x013D, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x013E, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x013F, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0140, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0141, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0142, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0143, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0144, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0145, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0146, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0147, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0148, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0149, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x014A, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x014B, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x014C, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x014D, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x014E, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x014F, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0150, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0151, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0152, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0153, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0154, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0155, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0156, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0157, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0158, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0159, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x015A, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x015B, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x015C, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x015D, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x015E, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x015F, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0160, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0161, 0x000C, 0x000C, 0x000C, 0x000C, 0x000C, 0x000C 0x0162, 0x080C, 0x080C, 0x080C, 0x080C, 0x080C, 0x080C 0x0163, 0x0110, 0x0110, 0x0110, 0x0110, 0x0110, 0x0110 0x0164, 0x4489, 0x4489, 0x4489, 0x4489, 0x4489, 0x4489 0x0165, 0x00C3, 0x00C3, 0x00C3, 0x00C3, 0x00C3, 0x00C3 0x0166, 0xE115, 0xE115, 0xE115, 0xE115, 0xE115, 0xE115 0x0167, 0x0D4A, 0x0D4A, 0x0D4A, 0x0D4A, 0x0D4A, 0x0D4A 0x0168, 0x0A96, 0x0A96, 0x0A96, 0x0A96, 0x0A96, 0x0A96 0x0169, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x016A, 0x2A4A, 0x2A4A, 0x2A4A, 0x2A4A, 0x2A4A, 0x2A4A 0x016B, 0x818A, 0x818A, 0x818A, 0x818A, 0x818A, 0x818A 0x016C, 0x0800, 0x0800, 0x0800, 0x0800, 0x0800, 0x0800 0x016D, 0x0800, 0x0800, 0x0800, 0x0800, 0x0800, 0x0800 0x016E, 0x318C, 0x318C, 0x318C, 0x318C, 0x318C, 0x318C 0x016F, 0x0095, 0x0095, 0x0095, 0x0095, 0x0095, 0x0095 0x0170, 0x0C0F, 0x0C10, 0x0C0F, 0x0C10, 0x0C0F, 0x0C10 0x0171, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0172, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0173, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0174, 0x000F, 0x0010, 0x000F, 0x0010, 0x000F, 0x0010 0x0175, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0176, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0177, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0178, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0179, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x017A, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x017B, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x017C, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x017D, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x017E, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x017F, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0180, 0x0752, 0x0752, 0x0752, 0x0752, 0x0752, 0x0752 0x0181, 0xC850, 0xC850, 0xC850, 0xC850, 0xC850, 0xC850 0x0182, 0x5326, 0x5326, 0x5326, 0x5326, 0x5326, 0x5326 0x0183, 0xA01E, 0xA01E, 0xA01E, 0xA01E, 0xA01E, 0xA01E 0x0184, 0xE976, 0xE976, 0xE976, 0xE976, 0xE976, 0xE976 0x0185, 0x19CF, 0x19CF, 0x19CF, 0x19CF, 0x19CF, 0x19CF 0x0186, 0x31D7, 0x31D7, 0x31D7, 0x31D7, 0x31D7, 0x31D7 0x0187, 0x0D9B, 0x0D9B, 0x0D9B, 0x0D9B, 0x0D9B, 0x0D9B 0x0188, 0x0CA9, 0x0CA9, 0x0CA9, 0x0CA9, 0x0CA9, 0x0CA9 0x0189, 0x0014, 0x0014, 0x0014, 0x0014, 0x0014, 0x0014 0x018A, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x018B, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x018C, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x018D, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x018E, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x018F, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0190, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0191, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0192, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0193, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0194, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0195, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0196, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0197, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0198, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0199, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x019A, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x019B, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x019C, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x019D, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x019E, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x019F, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01A0, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01A1, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01A2, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01A3, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01A4, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01A5, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01A6, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01A7, 0xF020, 0xF020, 0xF020, 0xF020, 0x0000, 0x0000 0x01A8, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01A9, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01AA, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01AB, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01AC, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01AD, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01AE, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01AF, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01B0, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01B1, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01B2, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01B3, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01B4, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01B5, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01B6, 0x600A, 0xA001, 0x600A, 0xA001, 0x600A, 0xA001 0x01B7, 0x0200, 0x0200, 0x0200, 0x0200, 0x0200, 0x0200 0x01B8, 0x0010, 0x0010, 0x0010, 0x0010, 0x0010, 0x0010 0x01B9, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01BA, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01BB, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01BC, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01BD, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01BE, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01BF, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01C0, 0x5C29, 0x5C29, 0x5C29, 0x5C29, 0x5C29, 0x5C29 0x01C1, 0xA829, 0xA829, 0xA829, 0xA829, 0xA829, 0xA829 0x01C2, 0x7E9E, 0x7E9E, 0x7E9E, 0x7E9E, 0x7E9E, 0x7E9E 0x01C3, 0xF3C6, 0xF3C6, 0xF3C6, 0xF3C6, 0xF3C6, 0xF3C6 0x01C4, 0x01C2, 0x01C2, 0x01C2, 0x01C2, 0x01C2, 0x01C2 0x01C5, 0x1C70, 0x1C70, 0x1C70, 0x1C70, 0x1C70, 0x1C70 0x01C6, 0x530B, 0x530B, 0x530B, 0x530B, 0x530B, 0x530B 0x01C7, 0xF1C1, 0xF1C1, 0xF1C1, 0xF1C1, 0xF1C1, 0xF1C1 0x01C8, 0x01C1, 0x01C1, 0x01C1, 0x01C1, 0x01C1, 0x01C1 0x01C9, 0xB1C1, 0xB1C1, 0xB1C1, 0xB1C1, 0xB1C1, 0xB1C1 0x01CA, 0x1600, 0x1600, 0x1600, 0x1600, 0x1600, 0x1600 0x01CB, 0x1600, 0x1600, 0x1600, 0x1600, 0x1600, 0x1600 0x01CC, 0x1000, 0x1000, 0x1000, 0x1000, 0x1000, 0x1000 0x01CD, 0x1241, 0x1241, 0x1241, 0x1241, 0x1241, 0x1241 0x01CE, 0x0555, 0x0555, 0x0555, 0x0555, 0x0555, 0x0555 0x01CF, 0x1708, 0x1708, 0x1708, 0x1708, 0x1708, 0x1708 0x01D0, 0x1313, 0x1515, 0x0014, 0x0014, 0x0000, 0x0000 0x01D1, 0x0909, 0x1515, 0x0000, 0x0000, 0x0000, 0x0000 0x01D2, 0x0904, 0x0904, 0x0000, 0x0000, 0x0000, 0x0000 0x01D3, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01D4, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01D5, 0xF500, 0xF500, 0xF500, 0xF500, 0xF500, 0xF500 0x01D6, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01D7, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01D8, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01D9, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01DA, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01DB, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01DC, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01DD, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01DE, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01DF, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01E0, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01E1, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01E2, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01E3, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01E4, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01E5, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01E6, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01E7, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01E8, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01E9, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01EA, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01EB, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01EC, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01ED, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01EE, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01EF, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01F0, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01F1, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01F2, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01F3, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01F4, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01F5, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01F6, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01F7, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01F8, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01F9, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01FA, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01FB, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01FC, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01FD, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01FE, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x01FF, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000 0x0200, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000, 0x0000
Question
Since after manual settings we applied in 1000BASE-T the ethernet link never comes up (after plugging the CAT5E cable between devices the link status is reported as link-down on both DP83867ISs), what is correct register settings sequence to achieve fast link-up time (30ms or better) with 1000BASE-T mode without auto-negotiation and with manual MDI and master/slave settings?
Thank You,
Cyril