Part Number: DS90UB940-Q1
Hi All,
Customer is using DS90UB949+DS90UB940 combination, and try to use the reverse SPI function, but still get the function to work, SOC has already sent CS/CLK/DATA to.940, but 949 is not outputing any signal.
According to my understanding, we only need to configure the HSCC_MODE of the two device to 111 to set the device in <high speed,reverse channel SPI mode>, but it doesn't work.
Could you please suggest any other register need to be configured? Thanks.
Best Regards
Charles Zhang