Part Number: TPS65981
Other Parts Discussed in Thread: TPS25740,
Hello All,
We are working on a new design with Galaxy S8 (as a host) and we using USB interface with it and the USB HUB (TUSB8044) by a Type C connector.
We need to add a Power Delivery for charging the phone so we can use charging and data transfer at the same time.
we already tested the TUSB321 and the TPS25740 and it's not working....
Now we'll try using the TPS65981, and we need to know how to connect the D+ D- from the USB HUB for data transfer with PD at the same time ?
Do I need to connect them directly to the TYPE C connector pins (A6,A7 / B6,B7) or do I need to connect them to the TPS65981 ?
Can you help me with a reference schematic ?
attached PDF - "HW_block diagram_Description" of our project.
We using just one type C connector, from the USB HUB to the phone.
All the rest connectors are type A USB connectors.
Thanks.