Part Number: SN7534051
I have two systems that need access to the same RS422 signal source. So, I wish to split the RS422 signal (running at a maximum of 5 MHz) into two (2) branches, and feed each branch to a different system. I have selected the SN7534051 chip. I am looking for a simple circuit diagram that shows if and how the inputs to the SN7534051 should be terminated. Also, I need to know if the outputs need any form signal management, or can they just be connected directly to the destination device?
Thanks,
Mo