This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TVS0500: limitation of SR<2.5V/us means it cannot be used for digital signal protection right?

Part Number: TVS0500

See title.

  • John-

    It depends on how fast the rise time of the digital signals are. Many times the rise time of digital signals are intentionally slowed down to help from an EMI perspective and our devices work perfectly, however they are not a good fit for fast switching signals like IOLink. A reminder that the slew rate limit in the datasheet is 1mA of leakage current ok, which is usually not a big impact to the system.

    If you have specific questions about an interface or an application, please email me at alec.forbes@ti.com and I can help you offline.

    Thanks,
    Alec