Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90CR485: My design is not working as expected

Part Number: DS90CR485

Is Pin 24 DC balance working in this part, the datasheet Figure 12 is label as GND?

If I connect pin 23 low do I only get data from channels A0P, A0M, A1P, A1M, A2P, A2M and A3P and A3M on rising edge of the clockin? Is the output data corresponding to input pins TxIN0 (D0) to TxIN23 (D23)?

I found the schematic for the demo board where pins 26, 27, 54, 59, 60, 61, 62, 63, 64, 65, 66, 67, 78, 88 are not connected. Is it OK to leave those pins floating?

When VCC3 is connected to 3.3V can pre-emphasis pin be connected with 50 ohms to 3.3V?

Thanks a lot for your help.

Roberto